This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCRC410EVM: FPGA development

Part Number: DLPLCRC410EVM
Other Parts Discussed in Thread: DLPLCR65NEVM,

Tool/software:

Hello Team,

Posting on behalf of my customer:

I do have DLPLCR410 and DLPLCR65NEVM. The mission is to realize a high-speed switching/refreshing as demonstrated in the introduction:
When paired with DLPLCRC410EVM, users get pixel-accurate control with 1-bit pattern rates up to 12,500 Hz.

However, I found it is not easy to use, as the GUI only supports ~10Hz. Someone suggested using FPGA by reading data from Sodimm, but I didn't see any introduction to address these. Can you give some
suggestions on it?

Regards,

Renan