Other Parts Discussed in Thread: DLP2000, DLP3010EVM-LC, DLPDLCR230NPEVM, DLP3010LC, DLPC3433
Tool/software:
Hi,
I've previously asked for settings for the DLPDLCR2000EVM to maximize fps, but imma start by saying I'm not sure whether it's the right Lightengine I want to use. I'll get back to that.
What i need is about 180-240 images per second. In equal intervals, Color is not so important, so my original idea was to use the 60Hz of the DLP2000 and simply split up my frame in RGB and boom tripled my framerate. That was before I learned that the EVM uses more than one Color cycle and the PMW signals to the LEDs aren't equally timed either. These are all settings for an optimal image under normal conditions, but that's not at all what I want to use it for. Also the image was bright enough to see but quite dark.
(Sidenote: I couldn't find any documentation about whether the DMD can operate under constant acceleration of around 10G (for example when mounted on a spinning object))
Due to the brightness and FPS limitations of the 2000EVM i was looking into other EVMs like for example the DLPDLCR230NPEVM and would like to buy a fitting one. I've also looked at Pattern projectors like the DLP3010EVM-LC which from the stats seem like what I want - fast pattern projection, but quite frankly extremely overkill and costly, so I would prefer the equal RGB split.
I've read what I could find of the documentation, but I don't want to make it unnecessarily costly, and want to find the minimum required hardware for the job. So 100+ lm would be nice but mainly I need a Pico projector capable of consistently projecting Patterns in high FPS and consistent RGB timings with one color cycle per frame and no Dark time.
So: 1. I need help determining the right hardware and whether it really fits my needs.
But then still remains the issue of programming it to have the equal timings and such. Since I hope to use DLP technology in the future for my product I think it's crucial for me to learn to properly deal with it. I've learned a lot by now, but I've studied mechanical engineering and don't have an entire embedded systems engineering degree, so I find it quite hard gathering together info piece by piece from high level documentations like the Programmers guide.
So 2. my second question would be whether there's a comprehensive guide or online course I can read/partake in in order to learn to handle these genius little machines, which picks up from a hobby-level programmer to a decent enough understanding. Also I've seen Software for easier i2C control for more expensive EVMs is there any chance to use it on the dlpc2000 or similar?
I've thought about embedded systems courses outside of texas instruments as well, but quite frankly I'm missing the terminology to even know what exactly I'm looking for, so a word of guidance on what to focus on to learn would be highly appreciated.
Sincere greetings