Other Parts Discussed in Thread: DLPC3470
Tool/software:
I am looking for a way to limit the inrush current during the startup of the DLPA2005.
It seems that a customized DLP firmware for current limiting has been provided in the DLP forum, so I would like to know if I can apply a similar solution.
The circuit diagram is as follows:
Only the Green LED is being used.
The current ripple during startup and normal operation is as shown below.
The desired current should not exceed 2A.
(Blue Line : Green LED
The firmware currently in use is:FWSel_DLPC3470_DLPA2005_pm2_i2c0x36_v9p2p0.img