This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCR4500EVM: How to project fast pattern in pattern sequence mode?

Part Number: DLPLCR4500EVM
Other Parts Discussed in Thread: DLP4500

Tool/software:

Hi, I am trying to project various vertical white line patterns within a very fast speed. (Approximately 120fps)

I am using pattern sequence mode, and I have uploaded the vertical white line images in 24 bitmap images using Firmware Upload tab.

But I am getting trouble when setting low value of Pattern exposure(us) and Pattern period(us). 

If I set these into a small value such as 66,000us for pattern period, the vertical line shows weird patterns.

The image below is the image of the weird pattern which is one of the frame of the vertical white line pattern sequence.



The picuture below is the correct pattern, when the Pattern exposure(us) and Pattern period(us) is defined as a large value such as 1,000,000 (us).


Could you help me what is wrong? Thank you.