Other Parts Discussed in Thread: DLP3010, DLPA2000
Tool/software:
Hello,
We're experiencing a problem with the DLPC3433 getting stuck on the splash screen during power on when the temperature is higher, but still within the declared operating limits. Depending on the chip it can sometimes be as low as 45C. The problem is very repeatable, ie a "bad" board will consistently get stuck at 55C while a good one can go above 70C and still boot up fine. The problem is very common, roughly half of the boards struggle above 60C.
The DLPC3433 is paired with DLPA2000 driving an off-board DLP3010 DMD.
The most recent test makes us think that the quality of individual DLPC3433 chips play significant role here:
we've swapped the DLPC3433 chips between two pairs of "good" and "bad" boards and on both of them the temperature performance followed the chip, so to say. So after the swap bad became good and vice versa.
We've realised that all the chips we have are from one batch - year 2021, week 24, and the foundry lot code, lot number etc are all identical as well.
Question - Is there any known issue in that batch? Has there been any newer batch/silicon revision released since then?