This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC3479: DLPC3479 Firmware for the external pattern mode using TI's basic FW

Part Number: DLPC3479


Tool/software:

Dear TI Members

In our existing the prvious scanner using DLPC3010, we utilized the default TI firmware, and we plan to apply the External Pattern Mode parameters to create our customized firmware for downloading and usage.

We are currently developing an External Pattern Mode based on the DLPC3479-DLPA3005-TIEVM-v8p4p0.img firmware.

Questions:

  1. When creating new firmware based on TI's firmware, will the DLPC3479-DLPA3005-TIEVM-v8p4p0'S firmware version remain unchanged?
  2. When creating new external firmware using TI's firmware, is it possible to use the Test Pattern Display functionality?