Tool/software:
Hello,
I have the DLP® LightCrafter 4500. I removed the leds to only keep the DMD for a microscopy illumination application.
I need to control it via Python so I found a few libraries, one being the cython hidapi (easily found on github). I checked their commands and they align well with the data sheets provided on your website pour the dlpc350.
Unfortunately, I'm having trouble connecting the controller via usb. I think it may be a driver issue. I can find my device on the Windows Device Manager, under "Universal Serial Bus Devices" with the name "DLPC350". However, when I search it via Python like that : hid.enumerate() , I only see the "DDP4421 Remote" device. As the DLPC350, it has VID_0451 and PID_6401, but it is MI_01 instead of MI_00 (this is what I should find for the DLPC350).
Also, it should be noted that I can apparently connect to the device with :
I don't understand what is happening or what I did wrong with the driver. I initially used the libusb-win32 driver for the PyCrafter4500 Python library. Then I changed it back to WinUSB with Zadig to use my new library.
Thanks in advance.
Chloe