Hello,
When in structured light mode with DVI input, there is the option to set the 'number of images per frame' anywhere from 1 to 24. This setting defines the bit-depth of the image. For example, setting it to 24 results in 24 monochrome images per frame while setting it to 3 results in 3 8-bit grayscale images per frame. However, I cannot find where the format of the 24-bit pixel value is defined for each of the 24 possible values for the 'number of images per frame' setting. Can anyone help me out?
Thanks,
Eric