This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4500: AR coating wavelength range/ no AR coating

Part Number: DLP4500


Tool/software:

I am using the DLP4500 chip in a desigh where we have wavelengths ranging from 500nm to 1000nm, especially the long wavelenghs are having problems due to the AR coating. We have looked at the NIR version but the fluctuatons in the AR curve at lower wavelengths wont work for us. Would it be possible to get the chip mounted with a window withouth AR coating ?  Are you  concidering a version with broadband AR that would cover a wider wavelengthrange ?

  • Hello Magnus,

    Regrettably at this time we are not considering a version of the chip with a wider wavelength range.  Any change such as this requires a significant validation process.

    What is it that you are trying to make?  Send me a friend invite if you wish to talk.

    Fizix