This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPLCRC900DEVM: technical assistance request (so#346922)

Part Number: DLPLCRC900DEVM
Other Parts Discussed in Thread: DLPC900, DLP9000

Tool/software:

Hi Tech,

P/N#DLPLCRC900DEVM

PO#029-ZX123

QTY:1

D/C: 2333 & Lot Code: 3013588SVT

Our customer used above board and met issue as below, please see attachment for details.

"When plugged into the computer, it reads out as DLPC670S instead of dlpc9000, and there is no initialization picture for DMD."

Could you help solve the problem?

Thanks.DLP9000 (so#346922).pptx

  • Hello Jun Liu,

    The DLPC900 Dual EVM User Guide has the instructions to program the flash image for a different DMD. Please refer to Section '4.10 Reprogram Controller Board for a Different Supported DMD' here.

    Customer can download the firmware for DLP9000 here and the GUI here.

    Thank you,

    Regards,
    Aishwarya