This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPA3005: Change 16A to 12A of the max current of LED

Part Number: DLPA3005
Other Parts Discussed in Thread: DLP4710, DLPC3479

Tool/software:

Hello TI,

Regarding DLPA3005, default configuration of max current is 16A. If we'd like to set the current = Max12A, should we change just RLIM(=12.5mΩ) value? Should we change other factors?(Such as parameters of the DLPC3429 firmware.)

Regards,

Uryyy