Tool/software:
Hi I hope someone out there can help with this.
What I think we need is a Corning Eagle XG Window or window glass piece. The windows we are trying to get are rated for UV pass through 350nm to 405nm, I think there are 2 different ones rated for UV. We just need the window glass preferably with the AR coating. Are these an Item that can be sourced? Or is there some kind of substitute glass that can be used even without the AR and even if it is oversized. What is the thickness of the window glass and what material is it. Does anyone know? We are not looking for the entire UV chip assembly as these are hard to get, even at any cost, availability is sketchy.
Thanks, much appreciated, Kevin