Tool/software:
Dear Texas Instruments Team,
Hello, I am currently developing a DLP-based 3D printer using the DLP670S chipset.
Since the DLP670S has a micromirror tilt angle of 17.5°, I have been illuminating the DMD with 405 nm UV light at a 35° incident angle, so that the reflected beam travels in the direction of the DMD surface normal.
While researching this setup, I came across the paper “Maximizing energy utilization in DMD-based projection lithography,” which suggests that the highest energy efficiency does not necessarily occur when the incident angle is twice the mirror tilt angle. Instead, the authors define a condition called the “blaze condition” that leads to maximum diffraction efficiency.
Based on this paper, I implemented a simulation and observed that the maximum efficiency occurs at an incident angle of approximately 46°, rather than at 35°.
This leads me to the following question:
Does Texas Instruments always consider and utilize the blaze condition when designing DLP projectors?
If not, could you please share the reason why this condition might be intentionally avoided or not prioritized?
Thank you very much for your time and support.
Best regards,
Minjae Kim