Tool/software:
Hello,
I am conducting experiments with the DLP3010EVM-G2 using the DLP EVM GUI, and the device selection in the GUI was set to DLP3010EVM-LC.
I mistakenly performed the action of writing the firmware of the DLP3010EVM-LC,
resulting in an error message "Error Details: Failed to write to I2C port via Cypress USB-Serial adapter" and I cannot read data from the EVM.
Even when trying to write the correct firmware for the DLP3010EVM-G2,
the same error appears and the issue does not improve. Is there any way to resolve this issue?