Other Parts Discussed in Thread: DLP780NE, DLP780TE, DLP781TE, DLP801XE, DLP801RE, , DLPC4420, DLPC4430, DLPA100, DLPA300, DLP9000XUV, DLPC4420AEVM, TMP411, DLP780NEEVM, DLP780TEEVM,
Tool/software:
Hello,
I have a question regarding most of the 0.78-0.8 inch DMDs (DLP801RE, DLP801XE, DLP800RE and DLP780TE, DLP780NE, DLP781TE):
Unlike for many other DMDs there is no wavelength range given for which these mirrors work. I am working at 2.6±0.1 micron and want to use the DMD for beam-shaping in an experiment. I assume the aluminum micromirrors should not be a problem (do they have any coating or is it just aluminum?) but is there any data/any restrictions from the window transmittance at these wavelengths?
And as a follow-up question: which components do I need to buy in addition to the DMD itself? I guess that I obviously need a controller (in this case 2x DLPC4420 or 1x DLPC4430, depending on which DMD I choose), a driver for power/motor (DLPA100) and a micromirror driver (DLPA300), is that correct? Apart from that, do I need to consider something specific as the LVDS for the input data?
Regards,
Miriam