Tool/software:
Hi Team,
I am using the P67 phase light modulation with DLPLCRC900DEVM with the GUI. When I upload the binary pattern image into the phase DMD, it works well. However, if 2-bit or higher bit image is uploaded, then it does not work.
This is the first time I’ve encountered an issue with the higher bits of the image. Although this is my first time using this EVM, I had no problems when using the DLPLCR6500EVM. Furthermore, with the DLPLCR6500EVM the GUI indicated DMD operation with an LED in the lower-left corner, but that indicator is not appearing now.
Any ideas on what might be causing the issue? Thanks in advance!
Kind Regards,
Jejomar