This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC4430EVM: HDMI connection

Part Number: DLPC4430EVM

Tool/software:

Good morning,

I would like to connect the Raspberry Pi to the EVM via HDMI. The Raspberry Pi has a micro HDMI output, but what kind of HDMI input is available on the EVM? What type of connector does it use?

Kind regards,

Miriam

  • Hello Miriam,

    The DLPC4430EVM kit come with a front end IT6802 board which has a standard HDMI connector. The part number of HDMI connector is10029449-111RLF on the front end board. 

    You can also refer to the DLPC4430EVM board design files. 

    Regards,

    Lori