This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDC4000 controller

Other Parts Discussed in Thread: DLP5500

Hi,

Can the DDC4000 controller work with the DLP5500. The DLP5500 has two 8 bit LVDS DDR data buses while the DDC4000 when used to drive the 0.55 DMD uses two 16 bit LVDS DDR data buses. I would like to develop a system that can use the slower DLP5500 or the more specialised and faster 0.55 and 0.7 DMDs


Thank you,

Liam

  • Hello Liam,

    Thank you for your post.

    I regret to inform you that the DDC4000 is not able to recognize the DLP5500 chip.  I understand the desire to make a flexible system that can do either, but at this time it is not possible with the DDC4x00 (4000 or 4100) architecture.

    If you have further questions please let me know.

     

    Fizix.