This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010EVM-LC: Temperature not reading after DLP firmware update.

Part Number: DLP3010EVM-LC
Other Parts Discussed in Thread: DLP3010, DLPC3478, DLPA2005

Tool/software:

Hello.

I am developing a product by customizing DLPC3478+DLPA2005+DLP3010.

I was using firmware version 8.0.1 well.
As shown in the figure below, you can see that the system temperature is read normally in version 8.0.1.

However, after updating to version 9.0.1 or 9.2.0, the system temperature continues to be read as 0. (See the figure below.)

What you need to know is that there is no hardware change at all.

When I only updated the FW, the problem occurred. Is this a problem caused by the FW change?

I installed all three versions of the GUI and checked them. (As shown in the figure.)

When reading with the 0xD6 command using the DLP API, the 8.0.1 version reads normally and the 9.2.0 version reads as 0..

Please let me know what is causing this issue.

**In addition, the picture below is the option I select when downloading the firmware.

I will wait for your reply.