Tool/software:
Please can you confirm the input port size for the DC barrel connector J2 as I can't see that listed on the datasheet. I believe it is 5.5mm OD x 2.5mm ID but wanted to confirm


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Please can you confirm the input port size for the DC barrel connector J2 as I can't see that listed on the datasheet. I believe it is 5.5mm OD x 2.5mm ID but wanted to confirm


Hello Jamie,
J2 is the power connector from CUI Inc. with part number PJ-082BH (Power Barrel Connector Jack 2.50mm ID (0.098"), 5.50mm OD (0.217") Through Hole, Right Angle).
You can find the HW design resources, including the BOM here - https://dev.ti.com/tirex/explore/node?node=A__AAc1l90yaHstn.AW6NWVbQ__DLP-AUTOMOTIVE-BOARDS__FUz-xrs__LATEST
Thank you,
Regards,
Aishwarya