Tool/software:
I'm using the DLPDLCR160CPEVM for my project, and I've installed the DLP EVM GUI for testing the board before proceeding.
After installing DLP EVM GUI 4.0.0.15 on my laptop, the software is not working; there is a process of the software running on the laptop, but the GUI never shows up.
I notice in the README file that this problem might be caused by a corrupted XML file, but I can't figure out which XML file in my installation folder is similar to the one in the instructions.
Is there a problem related to compatibility between Windows 11 and the software, and how can I fix this issue?
My system information:
OS: Windows 11 24H2
.NET Framework: 4.8
RAM: 20GB
CPU: Intel i5-11200H.