Tool/software:
Hi Friends,
I load the images in memory. It's working. but it loads the images very slowly to make it fast and load the images. and the image shows the time; that means the delay time. What is the maximum time to set?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Friends,
I load the images in memory. It's working. but it loads the images very slowly to make it fast and load the images. and the image shows the time; that means the delay time. What is the maximum time to set?
Hello User,
The load time is slow since the image has to be read from the card by the MCU and sent to the controller. There is not much that can be done to speed this process up to have the images show immediately.
I do not understand the request. Can you rephrase?
Best,
John
Hello User,
With default configuration the max delay between one SD card image to another is 50 seconds.
Bet,
John