Tool/software:
Hi~
How to Force ITE6807's Color Range Register to "Full Range" on an ITE6807+DLPC7540 Platform to Adapt to Front-End HDMI Signals.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ITE6807 controls color range via AVI InfoFrame. Critical registers:
0x0B (AVI InfoFrame DB2): Set to 0x010x0A (AVI InfoFrame DB1): Set to 0x02I want to know how to config these registers through DLPC7540 project.
Hello Jing,
Can you please point me to the registers table that you are referring to? Is this from ITE6807 datasheet that I could bot find the IT6807 datasheet online.
If this is from the frond end, then the controller DLPC7540 cannot set these registers.
You can also refer to the DLPC7540 software programmer's guide.
Regards,
Lori