Other Parts Discussed in Thread: DLP3010LC, , DLPC3478
Tool/software:
Hello,
I am seeking a suitable DMD eval module I need to be able to display and image for some specified number of milliseconds, and then swap to the next image in a sequence and repeat. I see that the DMD DLP3010LC supports: Pattern rate, binary (max) (Hz) 2487 - though I cannot find this in its corresponding datasheet. Further, the controller also supports: Pattern rate, binary (max) (Hz) 2487, but lists the maximum: Input Frame Rates up to 120 Hz. I am having a hard time understanding the difference between these specifications.
Simply put, does the evaluation module DLP3010EVM-LC support displaying binary images on the DMD at a rate of 1kHz using the provided firmware and software? Is there a minimum display/dark time for the evaluation module? I am only concerned with the DMD display, not any of the LED illumination aspects.
Thanks,
-Nathan