Tool/software:
Hi TI,
I am running an optical setup where I utilize both a DLP9000 and DLP6500 DMD on their evaluation boards for illumination patterning purposes. I previously used both boards with the EVM software on separate PCs, but I need to run both DMDs from a single PC. When I try to run multiple instances of the DLPC900REF-GUI to connect with each DMD or use a single instance to switch between the two components, I am unable to reliably connect to both DMDs. I am wondering if there is a procedure I should follow to simultaneously run both of these DMDs with a single PC, or if I need to use one PC per DMD module. Thank you in advance.
Best,
Alex