Tool/software:
Hi All,
Does the 64B/66B controller support
both the Framing Interface
and the Streaming Interface?
Looking at sections 7.3.1 and 7.3.1.1 of the TRM, it appears to send 64 DMD blocks
via an Aurora-compatible interface. However, native Aurora does not inherently signal DMD block boundaries, so it appears a mechanism using User-K is employed to indicate them (e.g., signaling the length?).
Therefore, regarding the Aurora data transfer specification for sending the DMD contents, it is unclear whether it is Streaming or Framing.
Best Regards,
Ito