Other Parts Discussed in Thread: DLP3030PGUQ1EVM, TPS99000S-Q1
Tool/software:
I am considering using automotive-grade DLP (DLP5530S-Q1 etc), for use in aircraft.
I have a few questions regarding this.
1. Storage Temperature
The storage temperature for the DLP is specified as -40°C, but some aircraft specifications require storage at -54°C. What potential issues might arise if stored at temperatures below -40°C?
2. Altitude
Some aircraft specifications require operation at altitudes of 50,000 ft or higher. Could altitude changes cause any problems? If possible, please provide any relevant data.
3. Sealing
Is the DLP completely sealed? If it is sealed, what type of gas is inside?
4. Vibration and Shock
Are there any specifications regarding vibration and shock ?
5. Flickering
We purchased the DLP3030PGUQ1EVM for evaluation. At room temperature, there were no issues, but at high temperatures (70-100°C), the image flickered occasionally. It didn't flicker constantly, but only intermittently. What could be the cause?