DLPC3479: Internal interrupt status of Read System Status (D1h)

Part Number: DLPC3479
Other Parts Discussed in Thread: DLPA3005

Tool/software:

Could you please provide details on the following?

Bit 3 of Byte 3 (Internal interrupt status) in Read System Status (D1h) in the DLPC3479 Software Programmer's Guide

I built a board using the DLPC3479 and DLPA3005.
The board is working fine.
However, one of the boards I have is not working.
When I check Read System Status (D1h), Byte 3 is 0x08.
The DLPC3479 Software Programmer's Guide states the following:
b(3) Reserved
'0': No Error '0': No Error
'1': Error '1': Error

  • Hello Koichi-sama,

    This indicates that bit index 3 is 1 (fourth bit), and as you noted is reserved.  This is not defined as to whether it is an error or not.  It is not defined.  Are there any other status bits that are different from the operating board you have?

    Fizix

  • Dear Fizix-san,

    Other registers and status bits are as follows:

    Read Short Status (D0h)
    Byte1 = 0x40, ... b(0,1,4,7) is unknown. This bit is masked out before displaying.

    Read System Status (D1h)
    Byte1 = 0x00
    Byte2 = 0x00, ... b(0,1,2) is unknown. This bit is masked out before displaying.
    Byte3 = 0x08
    Byte4 = 0x00, ... b(2,3) is unknown. This bit is masked out before displaying.

    Read Communication Status (D3h)
    Byte5 = 0x00, ... b(0,3) is unknown. This bit is masked out before displaying.
    Byte6 = 0x00

    The faulty board stops projecting the splash screen after a few seconds.
    Does this information suggest anything?

    Best Regards,
    Kadowaki

  • Hello again Koichi-sama,

    I need to consult with my colleague on this.  Please allow a day or two on this.

    Fizix

  • Hello Koichi-sama,

    Please advise what version of firmware you have programmed your board with.

    Additionally, you might be able to utilize these software and hardware debug tool - FAQ here.

    Best,

    Aaron

  • Dear Aaron-san,

    The firmware version is 8.4.1.
    I will try the debug tool.

    Best Regards,
    Kadowaki

  • Hello Koichi-sama,

    Your firmware is the latest, so there is no issue there.

    Let me know how the debug tool goes.

    Best,

    Aaron

  • Dear Aaron-san,

    A problem has been found in my host CPU control.
    The cause of the error in the DMDC status register (D0h, D1h) has not been identified, but it is possible that an internal pattern command was issued while in splash pattern mode.
    We apologize for the inconvenience.

    Best Regards,
    Kadowaki