This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP9500: Is the inside of the DLP9500's glass a vacuum or filled with inert gas?

Part Number: DLP9500


Tool/software:

TI Expert:

    Is the inside of the DLP9500's glass a vacuum or filled with inert gas?