Other Parts Discussed in Thread: DLP3010
Tool/software:
Hello Team,
We are working with the DLP3010 EVM and using structured binary patterns (black and white images, such as stripes). In the TI GUI, under Internal Trigger Mode, we can select one of the three illumination sources: Red, Green, or Blue.
When we upload a binary pattern (0 and 1), the selected illumination color is projected in the “1” portions of the image, while the “0” remains dark.
Our requirement is to project white light at the “1” portions of the binary image instead of only a single R/G/B channel. Could you please clarify how we can configure the GUI or EVM settings to achieve white light projection in internal trigger mode?
Regards
Abdul Basith
CDAC-T