This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Pico Kit V2 change default startup configurartion?



For the Pico Kit V2, is it possible to change the default start up configuration? We are working on an embedded application and the the Image Flip Long Axes to startup just the opposite from what it does not. We can change it with the Beagle board, but we need the changes to be made permanent. I assume the configuration defaults are stored in the flash PROM, is there a way to store new defaults in the flash PROM.

Thanks,

Tracy

  • Tracy,

    Welcome to the DLP & MEMS E2E forum.

    I understand your question. No, there is no provision for storing new defaults. The defaults are "hard wired" into the system code.

    It is possible to reprogram the system - that is, the hardware hooks are there. But this is not supported by TI. It would require access to the MSP430 code, which is not released.

    If you could tell me more about your project goals, we could perhaps suggest ways to achieve them.

    Best regards,

    Pascal