DLPDLCR471TPEVM: How to use the Debug pins (TSTPT_(7:0) ?

Part Number: DLPDLCR471TPEVM
Other Parts Discussed in Thread: DLPC6540

Tool/software:

Hi all,

I want to use the debug support function as described on page 70 of the DLPC6540 datasheet:

- On the EVM formatter board, these are on pins 2 through 9 of J6, correct?

- According to the datasheet, some test modes are accessible by setting TSTPT_3 to TSTPT_0 at powerup / reset, i.e. pulling up the pins which should be '1'. This does not work for me, all TSTPT_ pins are always low.

- The datasheet also states that the output selection can be reprogrammed by Software at any time. Is this possible through the I2C command interface?

Thank you in advance,

Matt