Other Parts Discussed in Thread: DLP6500FLQ, DLPC900
Dear Ti Team,
I'd like to purchase the DLP set you offer to stimulate a mouse's retina with a pattern.
I currently have a 532nm laser (fiber type) and would like to use additional optics to project the expanded laser onto the DLP (DMD) to stimulate the mouse's retina with the desired pattern.
If I purchase a DLP6500FLQ or DLP5500, can I create the pattern using the free software or SDK provided by TI without any additional equipment?
I'm wondering if the above-mentioned products are a single set. (I only need one DLP system.)
A brief schematic is shown below.
My biggest question is whether I can control the system by purchasing just one of the two products mentioned above.
(The product lines I've previously reviewed had separate controllers for the DMD and DLP, which was confusing.)
I need a complete set that includes a DLP system (with a DMD chipset) and a controller, without the need for a light source.
Best Regards,