This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How do you setup a trigger and sync with a camera?

The output trigger is provided for external camera synchronization.  There is option in the GUI to set the Trigger Pulse Width, Delay and Polarity settings.

The input trigger option is provided for pattern advancement in the pattern sequence. Multiple options exist for the input trigger:

     i. Command – Using software interface commands to select pattern

     ii. Auto – Automatically select the patterns

     iii. External – External hardware input signal both positive & negative edge Trigger

     iv. Camera – There is a camera port available on the System board, which can use the camera capture signal to trigger the pattern selection