Other Parts Discussed in Thread: DLPLCR65EVM
Dear TI E2E Support Team,
I am working with a DLPLCRC900EVM assembled with a DLPLCR65EVM (same configuration shown here). The LED is driven by an external driver.
My goal is to display a single pattern for 1 second, with all timing controlled by an Arduino. The sequence is:
-
t = 0 s: Arduino starts the trial
-
t = 1 s: Arduino enables the LED (5 V HIGH to the LED driver) and simultaneously sends a 3.3 V HIGH signal to Trigger 1 on the DLP board (J20) to display the pattern
-
t = 2 s: Trial ends
I have two questions (see the schematic attached; GND is not connected for scheme simplicity):
-
Is my triggering scheme complete as described in my printscreen? Do I also need to connect the LED enable signal to Trigger 2, or is using Trigger 1 sufficient for displaying a single pattern?
-
How long should the Trigger 1 signal remain HIGH to reliably initiate the pattern display? Is there a recommended minimum pulse width?
Thank you very much for your help.
Best regards,
Mariana