Other Parts Discussed in Thread: DLPC910, DLPC900, DLP9000XUV
Recently, we have the following requirements. We wonder if the DLPLCR4500EVM product can meet them. If it can, please see if specific operation suggestions can be provided.
Requirement It is necessary to generate red light vertical interference fringes of a certain area size (such as 40mm×40mm). Red light refers to light with a wavelength of about 635nm. This interference fringe has a certain period, such as an interference fringe spacing of 0.2mm to 1mm. Subsequently, CMOS/CCD and other photodetectors will be used to detect this interference fringe. In summary, it is necessary to generate red light interference fringes within a certain period.
If it can't be met, please help take a look at how to handle this application? Please give detailed suggestions. Thank you!