DLPLCRC410EVM: DLPCCRC410EVM: Please provide the SPI flash MCS and bit files for the FPGA and controller

Part Number: DLPLCRC410EVM
Other Parts Discussed in Thread: DLPC410

Hello, I am also facing the same issue and need the DLPC410 SPI Flash MCS and bit files for DLPLCRC410EVM

  • Hello Mingcheng,

    Thank you for coming to E2E! I've assigned this to a member of my team that is more familiar with this!

    Best,

    Aaron

  • Hello Mingcheng, 

    I just sent you a friend request through E2E. Please accept my friend request and I will send you the appropriate firmware files though there. In order to program the firmware (.mcs) files into the SPI PROMs correctly, you will need download a version of Xilinx Lab tools that support the XCF16 PROMs (Impact Tool v14.1). Additionally, please change the configuration to use the internal 40 MHz clock when programming the XCF16P SPI PROMs. Once firmware is successfully programmed,  D16 and D17 LEDs should be illuminated when the DLPLCRC410EVM is powered on.

    Best Regards, 

    Tristan Bottone