Hello,
I looked from the dlp5500 document (http://www.ti.com/lit/ds/symlink/dlp5500.pdf)
that the maximum illumination power density is :
-wavelength < 420 nm, 20mW/cm2
-wavelength > 700 nm, 10mW/cm2
But our biggest concern is VIS(480nm). I looked in the data sheet for the dlp5500 and followed the calculation in the page 19, so that maximum power density was estimated around 100W/cm2.The power density between VIS and UV(IR) is in a different class.Is calculated value reasonable?
I am looking forward to hearing from you.
Regards,
Kazuhiro