This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compatibility with external laser source (LightCrafter)



I want to replace the current light engine with a 780 nm laser. How reflective are the mirrors at this wavelength?

  • Hi Eldon,

    Welcome to TI DLP E2E Forum.

    The mirror surface reflectivity is 88% nominally for visible illumination (420-700nm). For 780nm wavelength, it is in between 86-87%. You have to be aware that TI does not guarantee the same performance beyond the values specified in the DLP3000 datasheet .

    Regards,

    Divya