Part Number: DLP3010
Hi Experts,
We are designing a projection system around DLP3010 for a medical device. We require quite a large amount of power trasmittance from a 894nm VCSEL array. Current estiamtes at the DMD are an average irradiance of ~500mw/cm^2 (a pulsed 30% duty cycle light). I see in the data sheet that the recomended limit is 10mw/cm^2 for any wavelength over 800nm but for 410-800nm it is much larger at 26.1W/cm^2.
Could you predict/calculate the maximum power for the DMD at specifically 894nm?
Regards,
Josel