Hello,
I would like to project a sequence of externally defined 24 bit .BMP images using the LightCrafter. My understanding is that a single 24 bit image can be projected while in 'Static Image Mode', or a sequence of images can be displayed as bit planes using 'Pattern Sequence' mode to project a single image. I've read in another forum post that an 'External Pattern' mode is on the way in a future LightCrafter software release.
Is there currently a way to project a small series (say 3-5) 24 bit images in sequence? If this feature will be added in a future software release, when do you expect that release?
Thank you for the assistance!
Sincerely,
Rob