Hey all,
my goal is to upload a couple of images / patterns to the DLP Light crafter and store them like an internal pattern and call the image like the internal patterns.
Is there any opportunity to add patterns to the internal patterns or is there any other solution present for this?
I also tried the sequence pattern but there is no possibility to use all three LEDs and also the exposure time is a problem there.
Is a solution created and saved in the GUI stored at the DLP Light Crafter?
In this case, is it possible to load such a solution by a command and the Light Crafter shows the image / pattern?
I am using Matlab to communicate with the DLP, at this moment I am able to set the display mode as well as set the internal patterns.
If it’s possible I want to avoid loading the image over Matlab -> a lot of HEX code.
Kind regards,
Andi