I did not notice this option in the DLP LightCrafter Control Software and I am wondering if this capability is present but just hasn't been implemented on this platform. I would like to create a static image (or a finite set of static images) and be able to apply an offset in both the x and y directions, to move the image across the display, horizontally and/or vertically. This option is much better than me having to store a series of shifted templates in memory to cover every possible location of that image, in a dynamic display.