I have a couple of question regarding the global reset phase of the DDC4100:
When using global reset-
1.Are no-op row cycles necessary after loading all rows and before initiating the reset, hence before switching BLK_MD = “11” and BLK_AD = “10XX”?
I'm aware that I have to send no-op cycles during RST-ACTIVE high, but should I also send no-op cycles after loading all the data and before initiating the reset?
This question is based on following quote from the DDC4100 - 2510443 document: "Following the loading of all rows in the device, a no-op row cycle must be completed to initiate the
reset."
2.Can you please comment on how long the values of BLK_MD and BLK_AD should be held to initiate the global reset, is one dclkin cycle enough?
Thanks in advance.