According to pg 31 of the User Guide:
Table 4-1. Trigger Connector Pins
DESCRIPTION | PIN | SUPPLY RANGE |
Trigger Supply | 1 | 3.3 V |
Trigger Input | 2 | 3.3 V |
Trigger Output | 3 | 3.3 V |
Ground | 4 |
3.3 V |
Are these 4 pins physically like this:
If I have a circuit look something like this: Pin1------------switch-------------Pin2
Would closing the switch issue a trigger signal?
In the software, under the "Pattern Sequence" tab, "Input trigger" is set to "External (Positive)." Shorting pin 1 and 2 produces no result but shorting pin 2 and 3 causes the pattern to change. Could someone help me explain why?
Also, "Exposure time" is set to 0 which according to the user guide would cause a pattern to be displayed until the next trigger signal is received. However, after shorting pin 2 and 3 briefly to change to a pattern, (at this point, pin2 and 3 are no longer shorted) that pattern only stay displayed for a few seconds and then the screen goes dark. Could someone help me explain this as well?
Thank you