This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDC4100 APPSFPGA OSERDES question



Hello,

My question relates to the APPSFPGA reference code,
I'm trying to understand the interface between the appcore module to the DDR OSERDES as I'm programming my own FPGA module.

I can see that the appcore_dout_x_q signals are 64 bits wide which are interleaved to 16 OSERDES cells using
(i,i+16,i+32,i+48) where 'i' is the i'th OSERDES cell.

My appcore design is using clk_g which is 100MHz. I shift in 64 bits of data to the appcore_dout_x_q registers and assert
the appcore_dout_valid right after, for one clk_g cycle.

I was wondering for how many clk_g cycles should the data stay stable in the appcore_dout_x_q register (64bits)
after the data_valid signal was asserted?

Thank you