Hello,
I'd like to display external 1-bit monochrome patterns with the LightCrafter at the maximum frame rate (24 * 60 Hz = 1440 Hz) and supply the "patterns" via HDMI. I don't care about the LEDs, since I will be using an external light source.
1) Is this possible?
2) If yes, can I get that by setting sending the TCP/IP command for "Video Mode Setting (0x02 0x01)"?
3) On page 28 of the LightCrafter users's guide it says "where this image enhancement is not desired, the video processing algorithms can be bypassed and replaced with a specific set of bit planes." How do I do that? I just want raw 1-bit images very fast, nothing else.
Thank you for your time!
-Gabriel