This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP Composer mass flashing or optimizing

Hello,

Is there a way to flash more than one unit at a time with DLP Composer or is there a way to optimize so we flash faster? We've gotten one computer's flash time down to around 3 minutes and our others average around 5. We need to bring this down to 2 minutes or less. This is for a complete image download. I'd appreciate any tips that could possibly help or share your flashing set up.

Thanks in advance for the help!

Chris

  • Chris,

    Welcome to the DLP&MEMS E2E.

    You will have to tell me more. What are you flashing? What is your application (or goal)?

    Best regards,

    Pascal

  • Thanks for the reply Pascal.

    We are using DLP Composer to update FW on projectors with a DDP2230. I'm trying to find a way to either decrease the time it takes to do a complete flash or if there is someway to flash the FW on more than one projector at a time with a single computer. Right now we can do 12 an hour per PC assuming there are no problems. I need around 15 an hour. We've tried running it on computers that are bare as far as software and such but did not see much change in flash time. 

    I'm assuming there's no way to flash multiple units because of not being able select which USB so I guess we are just looking for a way to optimize the flash time.

    Thanks,

    Chris