I acquired this from the surplus dept. But I found most of my questions answered online. except a major one.
When I power on the projector it just sits on the "dlp" splash screen. I have found in other forum posts to let it sit on for 10 seconds before it searches for input. so I tried that with the beagle board. Still nothing. different cables... nothing. hooked the BB up to a computer monitor to make sure it boots, resolution is correct, and it is. then tried to hook it up to my mac (dont have a pc with DVi) nothing... as I think the Ver1 doesn't have EDID...
So I also found in this forum, Gavin had his hang this way too, so I'm wondering if the person that used this before left it in a different video mode and I need to flash it via I2C and set it to the normal video mode. I have an arduino, and I have the ribbon to connect to it on the way from digikey...
Am I on the right track so far? or is this projector a dud?
any help would be greatly appreciated.