This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3-D Printing UV DLP Projector



Hi,

I am seeking information on getting a DLP projector that can output 385 nm wavelength or greater to cure UV resins for a 3-D printing application. I read that the conventional DLP projectors cannot handle these wavelengths as they degrade the DLP chip. I saw that the DLP Discovery 4100 kit can handle the appropriate wavelengths. However, from what I saw, this is just a chip set minus the lamp and optics for a projector. Are there any companies that sell a projector using the Discovery 4100 kit that can handle 385 nm wavelengths?

Thanks,

Sumontro